Figure 3-10 shows the
reset architecture of the AM263Px Control Card.
The AM263Px SoC has the following
resets:
- PORz is the Power-On-Reset for
the MAIN Domain.
- WARMRESETn is the Warm Reset to
MAIN Domain.
The PORz
signal is driven by a 3-input AND gate that generates a power on reset for the MAIN
domain when:
- The PMIC drives the NRES, MCU
Reset output signal low.
- The 1.2V buck regulator
outputs a low signal for the power good signal.
- The user push button (SW10)
is pressed.
- The Test Automation Header
outputs a logic LOW signal (TA_PORZn) to a P-Channel MOSFET gate which
causes V_GS of the PMOS to be less than zero and so the PORz signal connects
to the PMOS drain which is tied directly to ground.
The PORz signal is tied to:
- AM263Px SoC PORz input
- OSPI Flash Reset
- On-board Gigabit Ethernet PHY
reset
- Ethernet add-on board
connector
- BOOTMODE buffer output
enable
- High-Speed Edge Connector
(HSEC)
The WARMRESETn signal creates a warm
reset to the MAIN domain when:
- The user push button (SW12) is
pressed.
- The Test Automation Header
outputs a logic LOW signal (TA_RESETz) to a P-Channel MOSFET gate which causes
V_GS of the PMOS to be less than zero and so the RESETz signal connects to the
PMOS drain which is tied directly to ground.
The WARMRESETn signal is tied to:
- AM263Px SoC WARMRESETN
output
- RESETz signal created from push
button + PMOS logic
- IO Expander reset
- Micro SD reset
- HSEC
The AM263Px Control Card also has an
external interrupt to the SoC, INTn, that occurs when:
- The user push button (SW11) is
pressed.
- The Test Automation Header
outputs a logic LOW signal (TA_GPIO1) to a P-Channel MOSFET gate which causes
V_GS of the PMOS to be less than zero and so the INTn signal connects to the
PMOS drain which is tied directly to ground.