Microcontrollers (MCU)

Design Support

Getting Started

Selection Tool

Training & Events

Developer Network

University

 762 views

This application report enables easy migration from MSP430F2xx flash-based MCUs to the MSP430FR58xx/FR59xx/68xx/69xx family of FRAM-based MCUs. For the migration guide to MSP430FR57xx, see Migrating From the MSP430F2xx Family to the MSP430FR57xx Family. It covers programming, system, and peripheral considerations when migrating firmware. The intent is to highlight key differences between the two families. For more information on the use of the MSP430FR58xx/FR59xx/68xx/69xx devices, see the MSP430FR58xx, MSP430FR59xx, MSP430FR68xx, and MSP430FR69xx Family User's Guide. Although the MSP430F2xx and MSP430G2xx families are used as a base for comparison, similar considerations apply when migrating from MSP430F1xx and MSP430F4xx families.