SBOSAK2A May 2025 – September 2025 INA187
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The INA187 measures the differential voltage developed by current flowing through a resistor, commonly referred to as a current-sensing resistor or a current-shunt resistor. The INA187 can operate in either a unidirectional or bidirectional mode based on the voltage potential placed on the reference pin.
The linear range of the output stage is limited to how close the output voltage can approach ground as well the supply voltage as described in the Specifications. The value of the current-sensing resistor along with the current range to be measured, optimum gain option, as well as the voltage applied to the reference pin must be selected to keep the INA187 within the linear region of operation.