SPRS881K August 2014 – February 2024 TMS320F28374S , TMS320F28375S , TMS320F28375S-Q1 , TMS320F28376S , TMS320F28377S , TMS320F28377S-Q1 , TMS320F28378S , TMS320F28379S
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Figure 5-1 to Figure 5-4 show the terminal assignments on the 337-ball ZWT New Fine Pitch Ball Grid Array. Each figure shows a quadrant of the terminal assignments. Figure 5-5 shows the pin assignments on the 176-pin PTP PowerPAD Thermally Enhanced Low-Profile Quad Flatpack. Figure 5-6 shows the pin assignments on the 100-pin PZP PowerPAD Thermally Enhanced Thin Quad Flatpack.
![TMS320F28379S TMS320F28378S TMS320F28377S TMS320F28377S-Q1 TMS320F28376S TMS320F28375S TMS320F28375S-Q1 TMS320F28374S 337-Ball ZWT New Fine Pitch Ball Grid Array (Bottom View) – [Quadrant A] GUID-0211E546-5A82-4A3B-B030-815E089A4CD5-low.gif](/ods/images/SPRS881K/GUID-0211E546-5A82-4A3B-B030-815E089A4CD5-low.gif)
![TMS320F28379S TMS320F28378S TMS320F28377S TMS320F28377S-Q1 TMS320F28376S TMS320F28375S TMS320F28375S-Q1 TMS320F28374S 337-Ball ZWT New Fine Pitch Ball Grid Array (Bottom View) – [Quadrant B] GUID-FD11FF5A-5F95-4FFC-9591-9B68280683B6-low.gif](/ods/images/SPRS881K/GUID-FD11FF5A-5F95-4FFC-9591-9B68280683B6-low.gif)
![TMS320F28379S TMS320F28378S TMS320F28377S TMS320F28377S-Q1 TMS320F28376S TMS320F28375S TMS320F28375S-Q1 TMS320F28374S 337-Ball ZWT New Fine Pitch Ball Grid Array (Bottom View) – [Quadrant C] GUID-D27BCC18-A28E-433E-9299-2511D2A1578B-low.gif](/ods/images/SPRS881K/GUID-D27BCC18-A28E-433E-9299-2511D2A1578B-low.gif)
![TMS320F28379S TMS320F28378S TMS320F28377S TMS320F28377S-Q1 TMS320F28376S TMS320F28375S TMS320F28375S-Q1 TMS320F28374S 337-Ball ZWT New Fine Pitch Ball Grid Array (Bottom View) – [Quadrant D] GUID-5B9422A2-46E8-4217-B328-A635FA4A56F0-low.gif](/ods/images/SPRS881K/GUID-5B9422A2-46E8-4217-B328-A635FA4A56F0-low.gif)

The exposed lead frame die pad of the PowerPAD™ package serves two functions: to remove heat from the die and to provide ground path for the digital ground (analog ground is provided through dedicated pins). Thus, the PowerPAD should be soldered to the ground (GND) plane of the PCB because this will provide both the digital ground path and good thermal conduction path. To make optimum use of the thermal efficiencies designed into the PowerPAD package, the PCB must be designed with this technology in mind. A thermal land is required on the surface of the PCB directly underneath the body of the PowerPAD. The thermal land should be soldered to the exposed lead frame die pad of the PowerPAD package; the thermal land should be as large as needed to dissipate the required heat. An array of thermal vias should be used to connect the thermal pad to the internal GND plane of the board. See PowerPAD™ Thermally Enhanced Package for more details on using the PowerPAD package.
PCB footprints and schematic symbols are available for download in a vendor-neutral format, which can be exported to the leading EDA CAD/CAE design tools. See the CAD/CAE Symbols section in the product folder for each device, under the Packaging section. These footprints and symbols can also be searched for at https://webench.ti.com/cad/.