JAJSSH6 December 2023 MCT8315Z
PRODUCTION DATA
Because the output stages use N-channel FETs, the device requires a gate-drive voltage higher than the VM power supply to enhance the high-side FETs fully. The MCT8315Z integrates a charge-pump circuit that generates a voltage above the VM supply for this purpose.
The charge pump requires two external capacitors for operation. See Figure 8-1, Figure 8-2, Figure 8-3, Section 6 and Section 8.3 for details on these capacitors (value, connection, and so forth).
The charge pump shuts down when nSLEEP is low.