SBAU427 July 2025 ADS131E08
The ADS131E08 has an integrated voltage reference that provides a 2.4V or 4V reference voltage to the device. Alternatively, power down the internal reference and apply an external reference voltage on the VREFP pin of JP3. Apply the voltage reference externally by installing JP3 and providing the externally generated reference through JP3. Figure 2-4 shows the EVM circuitry for an external voltage reference (U3) such as the REF6241. The external voltage reference must be installed by the user. Set the external reference voltage between 2V and AVDD, depending on the analog supply voltage.