SLAAER4 March 2025 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
Figure 2-6 shows a simplified schematic of the V-to-I stage of the transmitter. This stage sets the current of the loop based on the voltage output of the DAC.
In this circuit, the DAC voltage is set across 120kΩ of equivalent resistance. The voltage at the opposite end of the 120kΩ is a virtual ground set by the feedback of the OPA333. The output of the OPA333 drives Q2 which sets the loop current.
The current flowing from VOUT, I1 combines with the current of I2. I2 is sourced from VREFIO across a 412kΩ resistor. This current contributes an offset to set the minimum current in the loop. The currents of I1 and I2 combine to set the voltage across a 20kΩ resistor below ground at LOOP–. The following equations show the voltage at LOOP–.
I1 and I2 are pulled from ground to LOOP–. Current through the 20kΩ resistor is amplified 1000:1 in the 20Ω resistor shown in I3.
The loop current is the sum of the currents through these paths and can be calculated as a function of I1 and I2.