SLAAER4 March 2025 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
The schematic in Figure 2-8 shows a simplified startup circuit of the HART transmitter.
When power is applied to the input terminals, voltage pulls up on LOOP+ to start up the circuit. Before Q1 turns on, the 12kΩ resistor supplies current to the 4.7V Zener diode. This voltage starts up the TPS7A0533 3.3V LDO. This LDO supplies the power to the AFE882H1 and OPA333 devices on the FE EVM board. As power is supplied to the AFE882H1, the current control of the EVM pulls base current from Q1 to set the current in the loop.