SLAAER4 March 2025 AFE781H1 , AFE782H1 , AFE881H1 , AFE882H1 , DAC8740H , DAC8741H , DAC8742H
The AFE882H1 front-end (FE) EVM is constructed as a field transmitter. The EVM uses a digital back-end board (DAC-FT-DBE) that connects to USB for control. The prototype versions of the two boards are shown in Figure 2-2.
Figure 2-2 AFE882H1 Evaluation Module with an
FTDI Digital-Back-End BoardIn the normal evaluation configuration, the board on the left is the DBE controller board. This board has a USB micro connection for computer control using a PC-based GUI. The DBE uses an FT4232H as the bridge between the USB and the digital communication with the AFE882H1. A 2x8 100mil connector joins the DBE board with the AFE882H1 FE EVM board.
The AFE882H1-FE-EVM board is shown on the right side of the figure. The board is constructed as a transmitter for a 4-20mA loop. The J6 terminal block on the right side board connects to an external 24V loop power supply. The current in the loop is set based on the DAC voltage output of the AFE882H1. When connected to the PC, the GUI sets the DAC output voltage and controls the current in the loop.
For this EVM, the board can be controlled by a GUI that can set the configuration of the device. The AFE882H1EVM GUI window is shown in Figure 2-3. The GUI is compatible with the AFE882H1-FE-EVM when connected to the DAC-FT-DBE.
Figure 2-3 AFE882H1EVM GUI Window