SLAU834 October 2020 ISO7760 , ISO7762 , MSP432E401Y , TPS92520-Q1 , TPS92682-Q1
This is a summary of the installation steps. To see step-by step instructions with screen shots, see Section 4.2.
Installation will take a few minutes, as it may need to install Microsoft®.NET Framework®. If the installer asks if you wish to reboot after installing Microsoft .NET, you must click Restart Later and allow the driver installation to complete.
After running the TPS92518, 520, 682 LaunchPad Evaluation Software Installer.exe, the evaluation software window appears as shown in Figure 4-1.