SPRAC21A June 2016 – June 2019 OMAP-L132 , OMAP-L138 , TDA2E , TDA2EG-17 , TDA2HF , TDA2HG , TDA2HV , TDA2LF , TDA2P-ABZ , TDA2P-ACD , TDA2SA , TDA2SG , TDA2SX , TDA3LA , TDA3LX , TDA3MA , TDA3MD , TDA3MV
This section provides a throughput analysis of the EDMA module. The enhanced direct memory access module, also called EDMA, performs high-performance data transfers between two slave points, memories and peripheral devices without microprocessor unit (MPU) or digital signal processor (DSP) support during transfer. EDMA transfer is programmed through a logical EDMA channel, which allows the transfer to be optimally tailored to the requirements of the application. The EDMA can also perform transfers between external memories and between Device subsystems internal memories, with some performance loss caused by resource sharing between the read and write ports.
The EDMA controller block diagram is shown in Figure 10. The EDMA controller is based on two major principal blocks:
The EDMA controller’s primary purpose is to service user programmed data transfers between internal or external memory-mapped slave endpoints. It can also be configured for servicing event driven peripherals (such as serial ports), as well. There are 64 direct memory access (DMA) channels and 8 QDMA channels serviced by two concurrent physical channels.
Figure 10. EDMA Controller Block Diagram DMA channels are triggered by external event, manual write to event set register (ESR), or chained event. QDMA are auto-triggered when write is performed to the user-programmable trigger word. Once a trigger event is recognized, the event is queued in the programmed event queue. If two events are detected simultaneously, then the lowest-numbered channel has highest priority. Each event in the event queue is processed in the order it was queued. On reaching the head of the queue, the PaRAM associated with that event is read to determine the transfer details. The transfer request (TR) submission logic evaluates the validity of the TR and is submits a valid transfer request to the appropriate transfer controller. The maximum theoretical bandwidth for a given transfer can be found by multiplying the width of the interface and the frequency at which it transfers data.
The maximum speed the transfer can achieve is equal to the bandwidth of the limiting port. In general, a given transfer scenario will never achieve maximum theoretical band width due to several factors, like transfer overheads, access latency of source/destination memories, finite number of cycles taken by EDMA CC and EDMA TC between the time the transfer event is registered to the time the first read command is issued to EDMA TC. These overheads can be calibrated by looking at the time taken to do a 1 byte transfer. These factors are not excluded in these throughput measurements.
The frequency and bus widths of the different memory and slave end points are summarized in Table 8.
| Module Name | Frequency (MHz) | Bus Width (bits) |
|---|---|---|
| EDMA TPTC+TPTC | 266 | 128 |
| L3 | 266 | 128 |
| OCMC RAM | 266 | 128 |
| EMIF | 266 | 128 |
| DSPL2 RAM | 600 | 128 |
| IVAHD SL2 | 388.33 | 128 |
| ICSS RAM | 200 | 32 |