SPRADP0 December   2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2-Q1 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1List of Acronyms
  5. 2Software Setup
  6. 3Hardware Setup
    1. 3.1 AM263x Connections
    2. 3.2 AM263Px Connections
    3. 3.3 Lauterbach® Connections
  7. 4Building MCU_PLUS_SDK Examples
    1. 4.1 CCS Import And Build
    2. 4.2 Command Line Build
  8. 5CMM Scripts
    1. 5.1 AM263x CMM Script
    2. 5.2 AM263Px CMM Script
  9. 6Flashing SBL Null
    1. 6.1 Using UniFlash tool
    2. 6.2 Using Command Line Python Scripts
  10. 7Debugging with Trace32 Software
  11. 8Summary
  12. 9References

Lauterbach® Connections

  1. Connect the Lauterbach adapter to the Dock board.
  2. Connect the Lauterbach trace probe to the same port (A or B) as on the adapter connected to the Dock board.
  3. Make sure the Trace probe and PowerView trace are connected properly to the adapter.
  4. Connect the JTAG cable between PowerView Trace and adapter.
  5. Connect the Lauterbach power supply to the PowerView trace and power on the hardware.
  6. Connect the Trace ribbon cable between the Trace probe and adapter.
 Lauterbach Setup
                    Connections Figure 3-5 Lauterbach Setup Connections
 Lauterbach Setup Connections Figure 3-6 Lauterbach Setup Connections

Now, users can power on the Lauterbach power supply.