SPRADP0 December 2024 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P2-Q1 , AM263P4 , AM263P4-Q1
This document provides a step-by-step guide to enable Lauterbach ETM Trace for Texas Instruments high-performance AM26x micro controllers. By following the hardware and software setup steps above and using the .cmm scripts with the Trace32 software, Lauterbach trace is enabled on the AM26x microcontroller. Figure 8-1 shows the trace for the GPIO LED blink example from the MCU_PLUS_SDK, running on the R5F Core-0, on the AM263P4 in OSPI boot mode.
Figure 8-1 Sample Trace Output