SPRK066 October 2025 F28377D-SEP
The production F28377D-SEP is rated to a total ionizing dose (TID) of 30 krad(Si). In the course of the SEE testing, the heavy-ion exposures delivered ≈10 krad(Si) per 107 ions/cm2 run. The cumulative TID exposure was controlled below 30krad (Si) per unit. All six F28377D-SEP devices used in the studies described in this report stayed within specification and were fully-functional after the heavy-ion SEE testing was completed.