SWRA370A September 2011 – December 2025 CC1100 , CC1101 , CC2500 , CC2510 , CC2520 , CC2530 , CC2530-RF4CE , CC2540 , CC2540T , CC2541 , CC2541-Q1
All the tests in this document use SmartRF Studio, and depending on the device, the device will use SmartRF Studio 7 or SmartRF Studio 8. This section briefly describes setting up the software after connecting the device to the PC with SmartRF Studio installed.
Note that some options in the software do not appear depending on the capability of the EM or launchpad being tested.