For conducted measurements, the device
under test (DUT) is connected to the tester via a 50Ω RF cable with SMA connectors. The
LaunchPad comes by default with the RF signal path routed to its PCB antenna. To re-route
the signal path to its SMA connector, a capacitor near this connector must be rotated by
90° on the board. This requires de-soldering it from its original position, rotating and
re-soldering it in the new position. Consult the LaunchPad user’ s guide for details.
For radiated measurements, the device
under test (DUT) must be connected to an antenna. Correspondingly, the spectrum analyzer
must have an antenna attached to its input. The LaunchPad comes by default with the RF
signal path routed to its PCB antenna and therefore does not require any modifications. If
an external antenna must be connected to the SMA connector, follow the procedure to rotate
the capacitor shown in the previous paragraph. Please note that radiated measurements are
typically taken within an anecoic chamber to prevent interference, and signal reflections,
which can cause inconsistent or inaccurate readings.
For RX testing, the input reference signal (both as the desired signal and the
interference signal) should have certain characteristics that must be set according to the
respective standards document.
Payload content of the desired signal should be a sequence specified by the relevant
standard. They must be identical for all transmitted packets.
In test cases where an interference signal is used, the interference signal
characteristics must be defined by the applicable standards for which the device is being
evaluated.