The table below lists the on-state functional
modes for the TPUL2G123-Q1.
(1) H = high voltage level, L = low
voltage level, X = don't care
(2) L = driving low, H = driving high,

= driving high for the
defined pulse width time,

= driving low for the
defined pulse width time
(3) These outputs are based on the
assumption that the indicated steady-state
conditions at the inputs have been set up long
enough to complete any output pulse.
(4) If an output pulse is triggered while a previous
output pulse is still active, the output continues
to drive high for one additional pulse width.