SCDS436A September 2023 – December 2024 TMUX9616 , TMUX9616N
PRODUCTION DATA
Latch-up is a condition where a low impedance path is created between a supply pin and ground. This condition is caused by a trigger (current injection or overvoltage), but once activated, the low impedance path remains even after the trigger is no longer present. This low impedance path may cause system upset or catastrophic damage due to excessive current levels. The latch-up condition typically requires a power cycle to eliminate the low impedance path.
The TMUX9616x is constructed on silicon on insulator (SOI) based process where an oxide layer is added between the PMOS and NMOS transistor of each CMOS switch to prevent parasitic structures from forming. The oxide layer is also known as an insulating trench and prevents triggering of latch up events due to overvoltage, fast voltage slew rates, and current injections. The latch-up immunity feature allows the TMUX9616x to be used in harsh environments. For more information on latch-up immunity, refer to Using Latch Up Immune Multiplexers to Help Improve System Reliability.