SCEA144 December 2024 LSF0101 , LSF0102 , LSF0108 , LSF0204
To maintain proper functionality of the internal FET of the LSF, the voltage biased at VREFA node needs to be the lowest voltage seen at the I/Os on A and B side. However, there can be cases where one of the I/Os operate lower than VCCA and that voltage rail is also unavailable. One example of this is when the input voltage at the I/O channels have a VOH,min that is substantially lower than VCCA for worst case conditions. To maintain that the FET operates in the proper state, VREFA needs to be biased to similar voltages as VOH,min to achieve signal integrity. One method of resolving this is to create a voltage divider network with the VCCA rail to maintain proper voltage at the VREFA node. For single supply operation with only VREFB rail, please refer to device data sheet.
Use 1MΩ for R1 to reduce leakage current.
Assume the below variables:
Then the below equation can be used to solve for R2 given known Vx:
Take an example where VREFA desired voltage is 1.4V but only a 1.8V power supply is available. In this case, we use R1= 1MΩ to reduce leakage and Vx to be 1.4V since it is the voltage required. Then the pulldown, R2 can be calculated through: