SCEA144 December   2024 LSF0101 , LSF0102 , LSF0108 , LSF0204

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1How Does the LSF000x Differentiate From the LSF010x During Setup?
  5. 2How is the Internal Body Diode of the LSF NMOS Configured?
  6. 3Are Pullup Resistors Required for Push-Pull Applications with the LSF?
  7. 4How is Power Consumption Calculated for LSF Devices?
  8. 5Can I use LDO as a Power Supply?
  9. 6What if my I/Os Operate Lower Than VREFA?
  10. 7Summary
  11. 8References

How is Power Consumption Calculated for LSF Devices?

The LSF Family translators use passive components to perform level translation therefore these devices do not consume much power on their own. Instead there are other areas where power is dissipated. One of which, is the small current that flows through the internal biasing FET of the device. During normal operation (LSF010x, LSF0204), there is a leakage current from VREB to VREFA as depicted in the Figure 4-1. This current can be calculated as ICC = (VREFB-VREFA-VTH)/ 200kΩ, where RBIAS is recommended to be a value of 200kΩ to minimize the leakage current from flowing back into VCCA.

 Leakage Current from Higher to Lower Power SuppliesFigure 4-1 Leakage Current from Higher to Lower Power Supplies

The second leakage current sinks into the driver side whenever an input low signal is being propagated through the device. During a logic LOW, the FET is turned on due to voltage difference between the source (driver) and the gate of the FET due to VGS > VTH. The FET operates similar to a small resistor, directly connecting the input to the output. During this time, there is current flow from RB1 on B side, through the FET, combining with the current flowing through pullup RA1 and sunk into the driver (AN) side.

 Leakage Current Into Driver Side During an Input Logic LowFigure 4-2 Leakage Current Into Driver Side During an Input Logic Low

The worst case is when all channels of the LSF device internal FET is on, where power dissipation, PD = N x ICH2 x RON where ICH is IB, the current flowing through the FET or VB/RB, and N is the number of channels actively switching. RON values can be used through data sheet values.

When a logic HIGH is being propagated, the FET transitions into cutoff mode, where the input and output are separated from one another, meaning negligible amount of current sinks back into the driver side (AN). The calculation of this leakage current is insignificant and can be disregarded during power consumption calculation.

 Leakage Current During an
                    Input Logic High Figure 4-3 Leakage Current During an Input Logic High