SLAAED1G May 2023 – August 2025 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0C1105 , MSPM0C1105-Q1 , MSPM0C1106 , MSPM0C1106-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1218 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3218-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0H3215 , MSPM0H3215-Q1 , MSPM0H3216 , MSPM0H3216-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1116-Q1 , MSPM0L1117 , MSPM0L1117-Q1 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1
TI manufactures a LaunchPad for one MSPM0 sub family with a superset MSPM0 on board. The same example code can be reused across this MSPM0 sub family. The nortos example is under the address mspm0_sdk_x_x_x_x \ examples \ nortos \ LP_MSPM0xxxx and the RTOS example is under the address mspm0_sdk_x_x_x_x \ examples \ RTOS \ LP_MSPM0xxxx. This section shows a brief introduction for some key example types.
In the RTOS example level, the most important folder is the Drivers folder that demos the peripheral control based on TI Drivers. In the Nortos example level, the most important folder is the DriverLib folder, which contains the peripheral example code based on DriverLib. The address and content example are shown in Figure 3-7.
Figure 3-7 RTOS and Nortos Code ExamplesFor reference, examples under Drivers and DriverLib supports all the platforms listed in Table 5-5. Examples under other folders at least support the CCS platform.
| Supported by SDK | Platform 1 | Platform 2 | Platform 3 | |
|---|---|---|---|---|
| IDE | CCS | Keil | IAR | |
| Compilers | TI Arm-Clang | GNU Arm (GCC) | Arm and Keil Compiler | IAR Arm compiler |
| RTOS | FreeRTOS | |||
| Code examples | DriverLib and TI Drivers | |||
For a MSPM0 peripheral quick start, see MSPM0 Academy. Tthis delivers training modules for various topics in the MSP MCU portfolio.