SLAAED1G May   2023  â€“ August 2025 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0C1105 , MSPM0C1106 , MSPM0C1106-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0H3216 , MSPM0H3216-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1117 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Overview
  5. MSPM0 Online Selection
  6. Software Development Instructions
    1. 3.1 Key Documentation
    2. 3.2 LaunchPad Setup
      1. 3.2.1 Debugger Selection
      2. 3.2.2 LaunchPad Introduction
    3. 3.3 MSPM0-SDK Setup
      1. 3.3.1 MSPM0-SDK Installation
      2. 3.3.2 MSPM0-SDK Introduction
        1. 3.3.2.1 Examples Folder Introduction
        2. 3.3.2.2 Documents Folder Introduction
    4. 3.4 SysConfig Setup
      1. 3.4.1 SysConfig Installation
      2. 3.4.2 SysConfig Introduction
        1. 3.4.2.1 Basic Concept
        2. 3.4.2.2 Project Configuration View
        3. 3.4.2.3 Board View
        4. 3.4.2.4 NONMAIN View
        5. 3.4.2.5 SYSCTL View
        6. 3.4.2.6 Peripherals Setup
    5. 3.5 IDE Quick Start
      1. 3.5.1 CCS Quick Start
        1. 3.5.1.1 CCS Installation
        2. 3.5.1.2 Import a SDK Example
        3. 3.5.1.3 Example Download and Debug
        4. 3.5.1.4 Migrating Between MSPM0 Derivatives
        5. 3.5.1.5 Generate Hex Files
        6. 3.5.1.6 Program NONMAIN
      2. 3.5.2 IAR Quick Start
        1. 3.5.2.1 Environment Setup
          1. 3.5.2.1.1 SDK Support Setup
          2. 3.5.2.1.2 SysConfig Support Setup
        2. 3.5.2.2 Import a SDK Example
        3. 3.5.2.3 Example Download and Debug
        4. 3.5.2.4 Migrating Between MSPM0 Derivatives
        5. 3.5.2.5 Generate Hex Files
        6. 3.5.2.6 Program NONMAIN
      3. 3.5.3 Keil Quick Start
        1. 3.5.3.1 Environment Setup
          1. 3.5.3.1.1 MSPM0 CMSIS-Pack Setup
          2. 3.5.3.1.2 Sysconfig Support Setup
        2. 3.5.3.2 Import a SDK Example
        3. 3.5.3.3 Example Download and Debug
        4. 3.5.3.4 Migrating Between MSPM0 Derivatives
        5. 3.5.3.5 Generate Hex Files
        6. 3.5.3.6 Program NONMAIN
  7. Hardware Design Instructions
    1. 4.1 Obtaining a MSPM0 Package
    2. 4.2 Fix Pin Functions through Sysconfig
    3. 4.3 Schematic and PCB Attentions
  8. Mass Production Instructions
    1. 5.1 Generate Production Image
    2. 5.2 Program Software Tools Quick Start
      1. 5.2.1 Uniflash Quick Start
        1. 5.2.1.1 Program Through SWD
        2. 5.2.1.2 Program Through Bootloader
        3. 5.2.1.3 Program Through CMD Line Interface
      2. 5.2.2 JFlash Quick Start
      3. 5.2.3 C-GANG Quick Start
    3. 5.3 Program Hardware Quick Start
  9. Quality and Reliability Instructions
    1. 6.1 Quality and Reliability Material Entrance
    2. 6.2 Failure Information Collection and Analysis Guidance
  10. Common Development Questions
    1. 7.1 Unlock MCU
      1. 7.1.1 Unlock Through Bootloader
      2. 7.1.2 Unlock Through Factory Reset GUI Tool
      3. 7.1.3 Unlock Through Uniflash
      4. 7.1.4 Unlock Through CCS
      5. 7.1.5 Unlock With Reset Pin Disabled
    2. 7.2 MSPM0 Program Failure
    3. 7.3 Attentions When Disabling SWD or REST Pin
    4. 7.4 MCU Performs Differently in Debug and Free Run
    5. 7.5 Set SWD Password
    6. 7.6 BSL Related Questions
    7. 7.7 Reach Expected Current in LPM Mode
    8. 7.8 CCS Common Questions
      1. 7.8.1 Change the Optimization Level
    9. 7.9 Keil Common Questions
      1. 7.9.1 Copy Keil Example Out of SDK
  11. Summary
  12. Technical Documentation Resources
    1. 9.1 Technical Reference Manuals
    2. 9.2 Subsystems
    3. 9.3 Reference Designs
    4. 9.4 Hardware EVM User's Guides
    5. 9.5 Application Briefs
    6. 9.6 Application Notes and Others
  13. 10Revision History

Program Hardware Quick Start

Due to J-Link is commonly used and C-GANG hardware is already introduced in Section 5.2.3, this section focuses on the XDS110 debugger. For more production programming tools, see E2E page.

There are four different types of XDS110 debuggers available. The summary table is listed Table 5-2.

Table 5-2 XDS110 Debugger Summary
Support Features XDS110 XDS110 On Board
TMDSEMU110-U MSPM0 LaunchPad LP-XDS110 LP-XDS110ET
JTAG Yes No Yes Yes
SBW Yes Yes Yes Yes
EnergyTrace Yes Rely on type No Yes
MSPM0 bootloader Yes Rely on type No No
Comment Highest Performance Cheapest Easy to use Easy to use

With the TMDSEMU110-U device, the pin that is used is shown in Figure 5-13. When using for bootloader, GPIOOUT0 must connect to the MCU reset pin. GPIOOUT1 must connect to the MCU invoke pin (PA18).

 Pin Connection of
                    TMDSEMU110-U Figure 5-13 Pin Connection of TMDSEMU110-U

For XDS110 on LaunchPad, the basic programming functions are intact compared to the TMDSEMU110-U. The board is shown in Figure 5-14. The cheapest XDS110 on LaunchPad is LP-MSPM0C1104. However, LP-MSPM0C1104 only supports SBW and there is no EnergyTrace or bootloader function.

 XDS110 Onboard Figure 5-14 XDS110 Onboard

LP-XDS110 and LP-XDS110ET are similar with XDS110 on a LaunchPad. The difference lies on that one has EnergyTrace function and the other does not. The pin assignment is shown in Figure 5-15.

For LP-XDS110 and LP-XDS110ET, the level shift function is enabled by changing the jumper at the left bottom of the board. The support voltage range is from 1.2V to 3.6V.

 LP-XDS110ET Figure 5-15 LP-XDS110ET