SLAAED1G May   2023  â€“ August 2025 MSPM0C1103 , MSPM0C1103-Q1 , MSPM0C1104 , MSPM0C1104-Q1 , MSPM0C1105 , MSPM0C1105-Q1 , MSPM0C1106 , MSPM0C1106-Q1 , MSPM0G1105 , MSPM0G1106 , MSPM0G1107 , MSPM0G1505 , MSPM0G1506 , MSPM0G1507 , MSPM0G1518 , MSPM0G1519 , MSPM0G3105 , MSPM0G3105-Q1 , MSPM0G3106 , MSPM0G3106-Q1 , MSPM0G3107 , MSPM0G3107-Q1 , MSPM0G3505 , MSPM0G3505-Q1 , MSPM0G3506 , MSPM0G3506-Q1 , MSPM0G3507 , MSPM0G3507-Q1 , MSPM0G3518 , MSPM0G3518-Q1 , MSPM0G3519 , MSPM0G3519-Q1 , MSPM0H3215 , MSPM0H3216 , MSPM0H3216-Q1 , MSPM0L1105 , MSPM0L1106 , MSPM0L1116 , MSPM0L1116-Q1 , MSPM0L1117 , MSPM0L1117-Q1 , MSPM0L1227 , MSPM0L1227-Q1 , MSPM0L1228 , MSPM0L1228-Q1 , MSPM0L1303 , MSPM0L1304 , MSPM0L1304-Q1 , MSPM0L1305 , MSPM0L1305-Q1 , MSPM0L1306 , MSPM0L1306-Q1 , MSPM0L1343 , MSPM0L1344 , MSPM0L1345 , MSPM0L1346 , MSPM0L2227 , MSPM0L2227-Q1 , MSPM0L2228 , MSPM0L2228-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Overview
  5. MSPM0 Online Selection
  6. Software Development Instructions
    1. 3.1 Key Documentation
    2. 3.2 LaunchPad Setup
      1. 3.2.1 Debugger Selection
      2. 3.2.2 LaunchPad Introduction
    3. 3.3 MSPM0-SDK Setup
      1. 3.3.1 MSPM0-SDK Installation
      2. 3.3.2 MSPM0-SDK Introduction
        1. 3.3.2.1 Examples Folder Introduction
        2. 3.3.2.2 Documents Folder Introduction
    4. 3.4 SysConfig Setup
      1. 3.4.1 SysConfig Installation
      2. 3.4.2 SysConfig Introduction
        1. 3.4.2.1 Basic Concept
        2. 3.4.2.2 Project Configuration View
        3. 3.4.2.3 Board View
        4. 3.4.2.4 NONMAIN View
        5. 3.4.2.5 SYSCTL View
        6. 3.4.2.6 Peripherals Setup
    5. 3.5 IDE Quick Start
      1. 3.5.1 CCS Quick Start
        1. 3.5.1.1 CCS Installation
        2. 3.5.1.2 Import a SDK Example
        3. 3.5.1.3 Example Download and Debug
        4. 3.5.1.4 Migrating Between MSPM0 Derivatives
        5. 3.5.1.5 Generate Hex Files
        6. 3.5.1.6 Program NONMAIN
      2. 3.5.2 IAR Quick Start
        1. 3.5.2.1 Environment Setup
          1. 3.5.2.1.1 SDK Support Setup
          2. 3.5.2.1.2 SysConfig Support Setup
        2. 3.5.2.2 Import a SDK Example
        3. 3.5.2.3 Example Download and Debug
        4. 3.5.2.4 Migrating Between MSPM0 Derivatives
        5. 3.5.2.5 Generate Hex Files
        6. 3.5.2.6 Program NONMAIN
      3. 3.5.3 Keil Quick Start
        1. 3.5.3.1 Environment Setup
          1. 3.5.3.1.1 MSPM0 CMSIS-Pack Setup
          2. 3.5.3.1.2 Sysconfig Support Setup
        2. 3.5.3.2 Import a SDK Example
        3. 3.5.3.3 Example Download and Debug
        4. 3.5.3.4 Migrating Between MSPM0 Derivatives
        5. 3.5.3.5 Generate Hex Files
        6. 3.5.3.6 Program NONMAIN
  7. Hardware Design Instructions
    1. 4.1 Obtaining a MSPM0 Package
    2. 4.2 Fix Pin Functions through Sysconfig
    3. 4.3 Schematic and PCB Attentions
  8. Mass Production Instructions
    1. 5.1 Generate Production Image
    2. 5.2 Program Software Tools Quick Start
      1. 5.2.1 Uniflash Quick Start
        1. 5.2.1.1 Program Through SWD
        2. 5.2.1.2 Program Through Bootloader
        3. 5.2.1.3 Program Through CMD Line Interface
      2. 5.2.2 JFlash Quick Start
      3. 5.2.3 C-GANG Quick Start
    3. 5.3 Program Hardware Quick Start
  9. Quality and Reliability Instructions
    1. 6.1 Quality and Reliability Material Entrance
    2. 6.2 Failure Information Collection and Analysis Guidance
  10. Common Development Questions
    1. 7.1 Unlock MCU
      1. 7.1.1 Unlock Through Bootloader
      2. 7.1.2 Unlock Through Factory Reset GUI Tool
      3. 7.1.3 Unlock Through Uniflash
      4. 7.1.4 Unlock Through CCS
      5. 7.1.5 Unlock With Reset Pin Disabled
    2. 7.2 MSPM0 Program Failure
    3. 7.3 Attentions When Disabling SWD or REST Pin
    4. 7.4 MCU Performs Differently in Debug and Free Run
    5. 7.5 Set SWD Password
    6. 7.6 BSL Related Questions
    7. 7.7 Reach Expected Current in LPM Mode
    8. 7.8 CCS Common Questions
      1. 7.8.1 Change the Optimization Level
    9. 7.9 Keil Common Questions
      1. 7.9.1 Copy Keil Example Out of SDK
  11. Summary
  12. Technical Documentation Resources
    1. 9.1 Technical Reference Manuals
    2. 9.2 Subsystems
    3. 9.3 Reference Designs
    4. 9.4 Hardware EVM User's Guides
    5. 9.5 Application Briefs
    6. 9.6 Application Notes and Others
  13. 10Revision History

Schematic and PCB Attentions

The minimum requirements (power, reset, and Vcore) with suggested values for MSPM0 hardware setup are shown in Figure 4-9.

  • Power pin: TI recommends adding 10uF and 0.1uF capacitors, which are used to remove AC noise on the power rail.
  • Reset pin: TI recommends adding a 47kR pullup resistor and a 10nF pulldown capacitor. This makes sure that the MSPM0 releases from reset, after the power rail is stabilized.
  • Vcore pin: This pin is used to stabilize the CPU voltage. For some MSPM0 devices, this pin is not included. If the pin is included, connect the pin to a 0.47uF capacitor.
 MSPM0 Minimum System Figure 4-9 MSPM0 Minimum System

Other considerations when drawing a schematic file are listed in Figure 4-10.

  • ROSC Pin: If users want to reach accurate high frequency clock with internal SYSOSC, then 0.1% resistor is suggested. Some low-cost devices cannot have this function.
  • VREF+/VREF- Pin:
    • If using an internal reference,then the G series require a 1uF capacitor between VREF+ and VREF- to support 4Msps ADC. For L or C series, then the capacitor is not required as the ADC speed is only support 200Ksps with internal Vref.
    • If using an external reference, then all the MSPM0 devices require a 1uF capacitor between VREF+ and VREF-.
  • Open-Drain IO: Open-Drain IO cannot output high voltage from the MCU side, so external pullup resistors are required, such as a 4.7kR capacitor.
  • Reset Pin: If reusing the reset pin as GPIO, I2C or UART, then the pullup resistor and the pulldown capacitor are still required. This makes sure that the MCU is released from reset state after the power is stable. TI recommends reducing the resistor and capacitor, such as using a 2.2kR pullup resistor and 10pF pulldown capacitor.
  • PA18: PA18 is the invoke pin to enter bootloader. Make sure this pin is not in pullup or affected by noise or analog signals with this pin floating. Otherwise, the device enters the bootloader instead of the application code. More details and a software option to change and disable the invoke pin in sysconfig are shown in Section 7.4.
 MSPM0 Schematic Figure 4-10 MSPM0 Schematic

For further information about schematics or PCB design references, see the following links.