SLAU958A January 2025 – March 2025 MSPM0G3507
This fault is triggered when the phase current is below the No motor lock threshold % of base current.
Step 1: Make sure the motor phases are connected to the terminals as shown in the Hardware User Guide.
Step 2: If the fault persists, decrease the No-Motor lock current threshold [NO_MTR_THR].