SLAU958A January 2025 – March 2025 MSPM0G3507
Initial Speed Detection (ISD) is a feature to enter the motor automatically when the motor is already spinning. This is also called Headwind/Tailwind startup, or Catch-on-the-fly startup. For basic spinning for motor, the ISD feature is disabled by default by setting isdEn = 0 on the Register Map page. For basic motor tuning, the motor is expected to be at standstill before giving the speed command. To tune the motor for ISD, see Section 7.
Figure 6-7 Disabling ISD in GUI