SLAU958A January 2025 – March 2025 MSPM0G3507
Driver propagation delay defines the Time delay in ns between the Input PWM logic edge fed to the gate driver and actual Gate Driver output. This delay impacts the Current Sense sampling instance on the actual gate driver output and has to be fed to the algorithm for accurate Current Sensing.
This value in ns has to be defined using #define DRIVER_PROPAGATION_DELAY_nS macro in the main,h file.