Whenever we need optimum handoff
(least time in open loop), use the following steps:
- For a proper handoff and to
accommodate variations in motor phase resistance/phase inductance (due to
temperature), the variables SPEED_REF_OPEN_LOOP and SPEED_FDBK on DAC needs to
match for 30% of the open loop time.
- Set OL_ILIMIT to Rated peak phase
current or ILIMIT.
- With OL_ACC_A2 = 0 (or the lowest
setting available). Set OL_ACC_A1 to next higher value of OL_ACC_A1 =
(MAX_SPEED/10)Hz/s. Verify whether handoff is proper or not. If the handoff is
not proper, revert to the previous setting else set OL_ACC_A1 to the next higher
value and continue this procedure.
- Now set OL_ACC_A1 at half of last
successful handoff setting, and now try increasing the value of OL_ACC_A2, until
we get a successful handoff.
- Set OPN_CL_HANDOFF_THR to the
next value higher than 20%. Verify whether handoff is proper or not. If the
handoff is not proper, revert to the previous setting else set
OPN_CL_HANDOFF_THR to the next higher value and continue this procedure.