SLLSFS6B September 2024 – October 2025
PRODMIX
In the pin mode, NFLT1 pin is driven low if the CQ driver enters overcurrent condition, or if the CQ driver temperature sensor has exceeded T(WRN). NFLT1 returns to high-impedance as soon as both the fault conditions clear.
Similarly, NFLT2 pin is driven low if the DO driver enters overcurrent condition, or if the DO driver temperature sensor has exceeded T(WRN). NFLT2 returns to high-impedance as soon as both the fault conditions clear.
If the LP supply or the VOUT supply fall below the UVLO thresholds, RESET pin goes low. RESET pin goes high after both LP and VOUT rise above the UVLO thresholds.