SLLSFS6B September 2024 – October 2025
PRODMIX
If the output current at CQ exceeds the internally-set current limit IO(LIM) for a duration longer than the current blanking time, tSC, the device detects the condition as an overcurrent fault.
In pin-mode, the INT/NFLT1 pin is driven logic low to indicate a fault condition. The output can be set to either turn off (auto-recovery mode) or continue to supply the current until the device enters thermal shutdown. The behavior depends on how the ILIM_ADJ1 pin is connected. See Table 7-2. In the auto-recovery mode, the driver periodically retries to check if the output is still in the over current condition. In this mode, the output is switched on for tSC in tAR intervals. Current fault auto retry mode can be disabled by setting ILIM_ADJ1 = OPEN or GND. Current fault blanking time is zero when ILIM_ADJ1=OPEN. See current limit indicator function (t > tSC) for details.
In SPI-mode, CQ_CURLIM register settings can be used to configure the CQ driver behavior. CQ_CUR_LIM bits set the current limit whereas the CQ_BL_TIME and CQ_RETRY_TIME set the current fault blanking time and auto-recovery time respectively. CQ_AUTO_RETRY_EN controls the auto-recovery behavior.
When the driver is disabled, the current limit indicator is inactive.