The I2C peripheral in MCF8329HS-Q1 implements clock stretching under certain
conditions when there are pending I2C interrupts waiting to be processed.
During clock stretching, MCF8329HS-Q1 pulls SCL low and the
I2C bus is unavailable for use by other devices. The following is a
list of conditions under which clock stretching can occur:
- Start interrupt pending:
There are two scenarios when a start interrupt can result in clock stretching,
- When target ID is a match, I2C
peripheral in MCF8329HS-Q1 raises a start
interrupt request. Until this start interrupt request is processed,
clock is stretched. Upon processing this request, clock is released and
an ACK (marked in yellow or grey in Figure 6-52 and Figure 6-53) is sent to the controller for continuing with the
transaction.
- If Start (followed by target ID match) for a new
transaction is received when a receive interrupt from previous
transaction is yet to be processed, clock is stretched until both the
receive interrupt and start interrupt are processed in chronological
order. This process maintains that previous transaction is executed
correctly before initiating the next transaction.
- Receive interrupt pending: When a receive
interrupt is waiting to be processed and the receive register is full which
occurs when two successive bytes (data or control) have been received by MCF8329HS-Q1 (separated by one ACK shown as blue boxes
in Figure 6-52 and Figure 6-53) without the receive interrupt generated by the first byte
being processed. Upon receive of second byte, clock is stretched until receive
interrupt generated by the first byte is processed.
- Transmit buffer is empty:
In case of a transmit interrupt pending (to send data back to controller), if
the transmit buffer is waiting to be populated with data to be read back to the
controller, clock stretching is done until the transmit buffer is populated with
requested data. After the buffer is populated, clock is released and data is
sent to controller.
Note: I2C clock stretching is timed out
after approximately 5ms by MCF8329HS-Q1 to allow
I2C bus access for other devices on the same bus.