SLUSG59 February 2026 BQ27Z855
ADVANCE INFORMATION
As stated in Section 7.2.2.2.2, choosing a sense resistor (RSENSE) value presents a tradeoff between the sense resistor value and the current resolution reported by the device's Coulomb counter for gauging calculations. This tradeoff is also present when the device's current limiter is enabled and impacts the current resolution the device senses and regulates charging current at.
This tradeoff is detailed as follows:
Using a combination of a particular sense resistor value and particular charging currents impacts the charging current resolution of the device since the device's battery charging functionality scales based on the sense resistor value.
In addition to the resolution, the sense resistor value also impacts the minimum charging current setting to achieve particular charging current accuracy. As a general guideline to achieve charging current accuracy of ±10%, the charging current settings programmed in device data flash is not recommended to be below the minimum values given in Table 7-2. Charging current settings below the recommended range when using a particular sense resistor value can still be programmed, but charging current regulated by the device may not be as accurate as ±10%. The charging current programmed in device data flash should also not exceed ICHG(MAX) as specified in the Current Limiter Specifications table. The combination of sense resistor value and charging current settings should be considered carefully then.
The sense resistor value's impact on charging current resolution and accuracy should be considered when programming the fast charge and precharge current settings in device data flash.
Table 7-2 provides guidance on how the sense resistor value impacts the charging current (ICHG) resolution and recommended range of the device:
| 0.5mΩ | 1mΩ | 2mΩ | 5mΩ | 10mΩ | 20mΩ | 50mΩ | 100mΩ | |
|---|---|---|---|---|---|---|---|---|
| ICHG Resolution (mA) | 29.30 | 14.65 | 7.32 | 2.93 | 1.46 | 0.73 | 0.29 | 0.15 |
| Minimum ICHG Setting (mA)(1) | 925 | 463 | 231 | 93 | 46 | 23 | 9 | 5 |
A lower termiantion current (ITERM) setting below the recommended ICHG range is allowed, but should not exceed ITERM(MAX) as specified in the Current Limiter Specifications table. Similar to the above general guideline to achieve ±10% ICHG accuracy, the ITERM setting programmed in device data flash is not recommended to be below the minimum values given in Table 7-3 to achieve ±10% ITERM accuracy. ITERM settings below the recommended range when using a particular sense resistor value can still be programmed, but the ITERM value detected by the device may not be as accurate as ±10%.
Table 7-3 provides guidance on how the sense resistor value impacts the ITERM resolution and recommended range of the device:
| 0.5mΩ | 1mΩ | 2mΩ | 5mΩ | 10mΩ | 20mΩ | 50mΩ | 100mΩ | |
|---|---|---|---|---|---|---|---|---|
| ITERM Resolution (mA) | 1.85 | 0.92 | 0.46 | 0.18 | 0.09 | 0.05 | 0.02 | 0.01 |
| Minimum ITERM Setting (mA)(1) | 55 | 28 | 14 | 6 | 3 | 1 | 1(2) | 1(2) |