SLUSG59 February 2026 BQ27Z855
ADVANCE INFORMATION
As stated in Section 7.2.2.2.1, the device measures cell voltage using the device's BAT pin. The measured cell voltage value provides the feedback needed for the device's current limiter to properly regulate charging current and charging voltage.
There are no additional external componenets required at the device's BAT pin to support the current limiter functionality besides the required components stated in Section 7.2.2.2.1.
In addition to the recommendation on the total resistance between CELL+ and the device BAT pin stated in Section 7.2.2.3.2, the following resistances should also be carefully considered to ensure proper charging and supplement mode behavior: