SLUUCG7 April 2024 BQ76922
| Class | Subclass | Name | Type | Min | Max | Default | Unit |
|---|---|---|---|---|---|---|---|
| System Data | Integrity | Config RAM Signature | U2 | 0x0000 | 0x7FFF | 0 | Hex |
Description: The lower 15 bits of the signature of static configuration options (which is returned by the STATIC_CFG_SIG subcommand) should be programmed into this parameter. When the STATIC_CFG_SIG subcommand is sent, the response will be checked against this value. If the value does not match, the top bit will be set in the response returned. This enables the system to validate the static config signature without having knowledge of the signature itself.