SLUUD68 December 2024
Figure 5-1 DESAT and Soft Turn-Off Waveform. This test is carried out without a bus voltage to test the functionality of DESAT pin, soft turn-off, and nFLT feedback.
The voltage on DESAT first reaches the detection threshold. After a short delay as specified in the UCC2189X5Y-Q1 data sheet, output experiences soft turn-off via the SSD pin. The soft turn-off current can be programmed by the resistor on SSD. On the primary side, nFLT also pulls low as a result of DESAT triggering, following a longer delay as specified in the datasheet.