Layout is critical for good power-supply
design. Layout example shows the recommended PCB layout configuration.
A list of PCB layout considerations using the device is listed as follows:
- Place the power components (including input and output capacitors, the inductor, and
the IC) on the top side of the PCB. To shield and isolate the small signal traces from
noisy power lines, insert at least one solid ground inner plane.
- PVIN-to-PGND decoupling capacitors are important for FET robustness. Besides the large
volume 0603 or 0805 ceramic capacitors, TI highly recommends a 0.1µF 0402 ceramic
capacitor with 25V / X7R rating on PVIN pin 20 (top layer) to bypass any high frequency
current in PVIN to PGND loop. TI recommends the 25V rating, but the rating can be
lowered to 16V rating for an application with tightly regulated 12V input bus.
- When one or more PVIN-to-PGND decoupling capacitors are placed on bottom layer, extra
impedance is introduced to bypass IC PVIN node to IC PGND node. Placing at least three
times PVIN vias on PVIN pad (formed by pin 20 to pin 24) and at least nine times PGND
vias on the thermal pad (underneath of the IC) is important to minimize the extra
impedance for the bottom layer bypass capacitors.
- In addition to the PGND vias underneath the thermal pad, at least 4 PGND vias are
required to be placed as close as possible to the PGND pin 7 to pin 10. At least two
PGND vias are required to be placed as close as possible to the PGND pin 19. This action
minimizes PGND bounces and also lowers thermal resistance.
- Place the VDRV-to-PGND decoupling capacitor as close as possible to the device. TI
recommends a 2.2µF/6.3V/X7R/0603 or 4.7µF/6.3V/X6S/0603 ceramic capacitor. The voltage
rating of this bypass capacitor must be at least 6.3V but no more than 10V to lower ESR
and ESL. The recommended capacitor size is 0603 to minimize the capacitance drop due to
DC bias effect. Make sure the VDRV to PGND decoupling loop is the smallest and make sure
the routing trace is wide enough to lower impedance.
- Place the VCC-to-AGND decoupling capacitor on the same side and as close as possible to
the IC. Connect VCC pin to VDRV pin with a 1ohm 0402 5% or better resistor. Placing a 1Ω
resistor between the VCC pin and VDRV pin forms a RC filter on VCC pin, which greatly
reduces the noise impact from power stage driver circuit. TI recommends a
2.2µF/6.3V/X7R/0603 or 4.7µF/6.3V/X6S/0603 ceramic capacitor. The voltage rating of this
bypass capacitor must be at least 6.3V but no more than 10V to lower ESR and ESL.
- For remote sensing, the connections
from the VOSNS/GOSNS pins to the remote location must be a pair of PCB traces with at
least 12 mil trace width, and must implement Kelvin sensing across a high bypass
capacitor of 0.1μF or higher. The ground connection of the remote sensing signal must be
connected to GOSNS pin. The VOUT connection of the remote sensing signal must be
connected to the VOSNS pin. To maintain stable output voltage and minimize the ripple,
the pair of remote sensing lines must stay away from any noise sources such as inductor
and SW nodes, or high frequency clock lines. And TI recommends to shield the pair of
remote sensing lines with ground planes above and below.
- For single-end sensing, connect the
VOSNS pin to a high-frequency local bypass capacitor of 0.1μF or higher, and short GOSNS
to AGND with shortest trace.
- The AGND must be connected to a solid
PGND plane. TI recommends to place two AGND vias close to the pin to route AGND from top
layer to bottom layer, and then connect the AGND trace to the PGND vias (underneath IC)
through either a net-tie or a 0Ω resistor on the bottom layer.
- Connecting a resistor from PMB_ADDR pin
to AGND sets the address. Do not to have any capacitor on this pin. A capacitor on the
pin likely leads to a wrong detection result for address.
- When the device is configured with an
external voltage divider, the high side resistor connects from VOSNS to VSEL/FB pins and
the low side feedback resistor connects to VSEL/FB to GOSNS pins near the device.
- The return for the MSEL1 resistor,
MSEL2 resistor, PMB_ADDR resistor, and VSEL/FB resistor (when using internal feedback
divider) is the quiet AGND island.