SLVSI23A September 2025 – December 2025 DRV81646
PRODUCTION DATA
The DRV81646 offers an INRUSH mode which boosts the current limit for a 10ms interval (tINRUSH) to support capacitive loads such as lamps which require a large current at turn on. To enable INRUSH mode, leave the COD/INRUSH pin unconnected or put a pulldown resistor larger than or equal to 1MΩ on the pin.
The current limit during tINRUSH is IINRUSH = 120 ÷ RILIM[kΩ] for RILIM≥ 40kΩ. This is also equal to 2 times the ILIM current limitation value. IINRUSH_ACTIVATE = IINRUSH + 50%, or
For example, a 60kΩ resistor on the ILIM pin results in IINRUSH = 120 ÷ 60 = 2.0A. The inrush current regulation only activates after the current passes IINRUSH_ACTIVATE = 2.0A × 1.5 = 3.0A. After 10ms the current is regulated at the ILIM level. Figure 6-11 shows the inrush behavior followed by regular ILIM current regulation until thermal shutdown or until the current drops below the ILIM level.
Figure 6-11 Current Limit Value During
INRUSHIf a channel shuts off during tINRUSH due to thermal shutdown, the inrush timer is paused until the channel temperature falls to a safe level, below TTSD-TTSD_HYS. Then the timer continues with the boosted current limit IINRUSH. The inrush timer count is reset if the corresponding INx is pulled low. When INx is pulled high the inrush counter restarts. Figure 6-12 illustrates this timer functionality with a load that causes a thermal shutdown during tINRUSH, and the current regulation dropping down to the ILIM setting after t > tINRUSH.
During tINRUSH, the nFAULT pin and NFAULT SPI bit is masked for that channel to prevent unwanted fault trigger during the initial inrush period. The nFAULT pin and bit still reports a fault on a different channel. For example, if Channel 1 is within tINRUSH and Channel 3 has a thermal shutdown, the nFAULT pin and bit report a fault.
| DEVICE STATE | CURRENT LIMIT | nFAULT PIN | FAULT BIT (SPI) |
|---|---|---|---|
| t < tINRUSH | IINRUSH | Masked during Inrush period tINRUSH | The FAULT bit of the corresponding channel is masked during Inrush period tINRUSH . |
| t > tINRUSH | ILIM | Pulled low if a power stage hits thermal shutdown. Released when channel temperature returns to a safe level. | The FAULT bit of the corresponding channel is set if channel hits thermal shutdown. The bit is cleared automatically at the end of valid SPI transaction |