SLVSJC6 December 2025 TPS544B27W
PRODUCTION DATA
The TPS544B27W supports the SMB_ALERT# response protocol through the Alert Response Address (ARA). The ARA response protocol is a mechanism by which the target device can alert the bus host about important information. The host can process this event and simultaneously accesses all target devices on the bus that support the protocol through the alert response address. All target devices asserting SMB_ALERT# acknowledge this request with the respective PMBus Address.
When a target device responds to the ARA, the device deasserts SMB_ALERT# but retains the offending status bits. After this successful notification, handling the interrupt becomes the responsibility of the host. The bus controller performs a modified receive byte operation to get the address of the target device, then uses the PMBus status commands to query the target device that caused the alert.
If multiple devices are asserting SMB_ALERT# low, the target device with the lowest address wins communication rights. If the SMB_ALERT# pin remains asserted after a successful receive byte operation using ARA, the host can query the ARA again to determine the next offending device.
To re-enable SMB_ALERT# triggering for initial fault sources (including any that occurred between SMB_ALERT# assertion and the ARA response), the original faults in the TPS544B27W must be cleared. This can be done by either:
For more information on the SMBus alert response protocol, see the system management bus (SMBus) specification.