SLVSNG2 August 2026 DRV8378-Q1
PRODUCTION DATA
The current-limit circuit activates if the current flowing through the low-side MOSFET exceeds the ILIMIT current. This feature restricts motor current to less than the ILIMIT.
The current-limit circuitry utilizes the current sense amplifier output of the three phases compared with the voltage at ILIMIT pin. shows the implementation of current limit circuitry. As shown in , the output of current sense amplifiers is combined with star connected resistive network. This measured voltage VMEAS is compared with the external reference voltage VILIM pin to realize the current limit implementation. The relation between current sensed on OUTX pin and VMEAS threshold is given as:
where
During the brake operation, a high-current can flow through the low-side FETs which can eventually trigger the over current protection circuit. This allows the body-diode of the high-side FET to conduct and pump brake energy to the VM supply rail.