The TPS55285EVM board can be enabled
to work by the following steps:
- Turn on the power supply.
- If Vin>5.1V, put JP2 in the ON
position to enable the output. If Vin<5.1V, connect EN to an external 3V
power supply or adjust R3, R6 resistor values to enable the output.
- Open the TPS55285EVM GUI.
- Click the auto connect button on
the target address widget (Figure 3-2). This automatically checks for target addresses (0x74, 0x75) and connect the
GUI with the device. After the GUI and device are connected, the GUI reads all
eight registers and shows a notification (Figure 3-3).
- Click the start button. This
shows the GUI user interface of TPS55285EVM-053 (Figure 3-4).
- Click the Enable button (Figure 3-5). The default output voltage is 5V.
- Set the output voltage, current
limit point, and so forth according to the design target. If the maximum load
current is ≥ 5A, then uncheck the Enable Current Limit check box or
increase the current limit value (Figure 3-6).