SLVUDB5A June 2025 – November 2025
Use the following instructions to perform the output hot short test:
| VIN = 54V, RIMON = 5.6kΩ, RIREF = 40.2kΩ, RSFT = 150kΩ, and COUT = 100uF |
Obtaining repeatable and similar short-circuit testing results can be difficult. The following factors contributes to the variation in results:
The actual short exhibits a certain degree of randomness because the short microscopically bounces and arcs. Verify that the configuration and methods are used to obtain realistic results. Hence, do not expect to see waveforms exactly like the waveforms in this user's guide because every setup is different.