Use the following instructions to
perform the persistent over-current test on the TPS1686 eFuse:
- Configure the jumper J2 position
to the desired reference voltage for overcurrent protection as mentioned in
7.
- Configure the Jumper J5 position
to set the required scalable fast-trip threshold (ISFT) as per 7.
- Set the input supply voltage VIN
to 54V and the current limit of 15A.
- Connect the power supply between
VIN2 (connector J13) and PGND (connector J11) and enable the power supply.
- Apply an overload in the range of
IOCP <ILOAD <ISFT between VOUT2
(connector J14) and PGND (connector J12) for a time duration more than
tTIMER decided by using jumper J3.
- Observe the waveforms using an
oscilloscope.