Comply with the following instructions
to measure the inrush current during a hot plug event:
- Configure the jumper J4 position to the desired start-up slew
rate as detailed in 7.
- Connect the positive terminal of the power supply to
connector J13.
- Connect the negative terminal of the power supply to connector
J11.
- Set the input supply voltage VIN to 54V and current limit to
10A. Enable the power supply.
- Observe the waveforms at VOUT2(TP38) and input current using an
oscilloscope to measure the slew rate and rise time of the VOUT2 with a given
input voltage of 54V.