SLVUDB9 July 2025
Before beginning to program the ADC EVM, you must first launch the GSPS FPGA SERVER to allow for programming and data capture. This can be done by launching the application by searching for GSPS_FPGA_Server in windows search bar and launching. Once this is done a console window with the following message seen in Figure 3-1. If this message is not seen, see Section 4 for assistance.
Figure 3-1 Server Listening for
ConnectionsOnce the server is launched, it does not have to be interacted with directly. All necessary communication happens via the ADC GUI.