SLVUDB9 July 2025 ADC34RF72
For programming, the ADC3xRF72 comes with a GUI that allows the user to configure the EVM into their desired mode of operation. The GUI can be found at the product page for the EVM on ti.com. Launch the GUI.
Figure 3-3 Sim Mode Not SupportedIf the ADC EVM successfully connects to the GUI, it looks like Figure 3-4. The GUI comes preset to a default configuration of Sampling frequency = 1.5GHz and all internal digital signal processing bypassed. If the hardware is configured as mentioned in Section 5, then the user can simply click "program ADC" and the GUI programs the ADC, the FPGA and tries to initialize the FPGA link so that data can start to be captured. Progress can be monitored in the below message console. If the ADC successfully programs the message, “ADC programming Success!” prints out in the console. Now the GUI starts to program the FPGA, debug messages can be seen in the message console as well but progress can also be monitored in the FPGA tab of the GUI. If the FPGA is successfully programmed and the link is successfully initialized then the following status shows in the FPGA tab. If not, then refer to Section 4 for further support.
Figure 3-4 EVM GUI Program ADC
Figure 3-5 ADC GUI FPGAIf the status matches what is shown in the figure, then the data can be captured and plotted in HSDC Pro. To do this press the “Capture Data” button in the ADC GUI. The resulting data can be seen in HSDC Pro as shown in Figure 3-6.
Figure 3-6 Example FFT Output
Spectrum