The MCF8329HSRRYEVM requires a power
supply source, which has a recommended operating range from a 4.5V to 60V. To setup
and power the EVM, follow the following sequence:
- Connect motor phases to A, B, and
C on connector J11.
- Do not turn on the power supply
yet. Connect the motor supply to PVDD and GND on connector J10.
- Select J7 to 5V_USB and J8 to
3V3COM to power MSP430 from USB power supply.
- Connect the micro-USB cable into
the computer.
- Turn the potentiometer fully
counter clockwise to set the motor to zero speed upon power up.
- Flip the switch S2 to the top to
configure DRVOFF = ON, and switch S4 to the bottom to configure WAKE.
- Set the Jumper J13 to the POT
position to apply the analog voltage from potentiometer R47 to the SPEED/WAKE
pin.
- Turn on the motor power
supply.
- Use the potentiometer R47 to
control the speed of the motor and the switches to disable the motor driver.
Optionally, use the GUI to monitor the real-time speed of the motor, put the
MCF8329HS into a low-power sleep mode, and read the status of the LEDs.