The eZ-FET Debug Probe on the MSP430FR2355
LaunchPad development kit uses a Spy-Bi-Wire JTAG interface to program the MSP430FR2355 MCU
on the MCF8329HSRRYEVM. Consult the MSP430 Launchpad Development Kits for MSP430 Launchpad development
kit to include an onboard eZ-FET Debug Probe.
- Remove the GND, 3V3, SBWTDIO, and SBWTCK jumpers
from the MSP430 LaunchPad development kit.
- Connect the top pins on the eZ-FET side of the
LaunchPad development kit of the GND, 3V3, SBWTDIO, SBWTCK signals to the respective pins
on J5 of the MCF8329HSRRYEVM as shown in Table 3-1 and Figure 3-3.
- Connect a micro-USB cable to the MSP430 LaunchPad
development kit and the PC.
- Click on the Build Project icon or CTRL+B to make sure the project builds successfully. Accept any updates if needed from the console
- Click on Debug Project to set up a debug session and press the Play button to run the code.
- Stop the debug session, close Code Composer
Studio IDE, disconnect the Spy-Bi-Wire jumpers, and unplug the micro-USB cable from the
MSP430 LaunchPad development kit.
Table 3-1 Spy-Bi-Wire Connections Needed to Program the MSP430FR2355| MSP430 LaunchPad™
Development Kit (eZ-FET Debug Probe Side) (J101) | MCF8329HSRRYEVM 4-pin
Spy-Bi-Wire Header (J5) |
|---|
| GND | GND |
| 3V3 | 3V3 |
| SBWTDIO | SBWTDIO |
| SBWTCK | SBWTCK |