SNOU210 November   2024

 

  1.   1
  2.   Description
  3.   Get Started
  4.   Features
  5.   Applications
  6.   6
  7. 1Evaluation Module Overview
    1. 1.1 Introduction
    2. 1.2 Kit Contents
    3. 1.3 Specification
    4. 1.4 Device Information
  8. 2Hardware
    1. 2.1 Overview
    2. 2.2 Perforations and Connectability
    3. 2.3 Status LEDs and Sub-regulator
    4. 2.4 Remote Sensor
    5. 2.5 Package Swapping
    6. 2.6 Power Supply
    7. 2.7 Programming Header
    8. 2.8 BSL Button
  9. 3Software
    1. 3.1 Software Download
      1. 3.1.1 Live Software on dev.ti.com
      2. 3.1.2 Offline Software
        1. 3.1.2.1 Download From dev.ti.com
    2. 3.2 Home Tab
    3. 3.3 Information Tab
    4. 3.4 Data Tab
    5. 3.5 Registers Tab
    6. 3.6 Collateral Tab
  10. 4Hardware Design Files
    1. 4.1 Schematic
    2. 4.2 PCB Layouts
    3. 4.3 Bill of Materials
  11. 5Additional Information
    1. 5.1 Trademarks

Overview

The EVM is divided into 2 sections: the controller section and the breakable sensor section. The sensor breakout section can be detached to use the sensor in the following scenarios:

  • Using the controller section with the sensor section connected by soldered wires/connectors to evaluate the sensor far from the controller and PC at extreme temperatures or other conditions.
  • Using the sensor section with the user's system by interfacing with the TMP411 using SMBus communication protocol.
  • Using the controller section with TMP411 sensors in the user's system.

Figure 2-1 highlights the EVM sections as well as some components that must be identified by the user to understand the purpose and use. The components are further explained in detail in the sections below.

TMP411 TMP411EVM Board SectionsFigure 2-1 TMP411EVM Board Sections
TMP411 TMP411EVM Bottom SideFigure 2-2 TMP411EVM Bottom Side