SNOU210 November 2024
The Data tab reports the temperature measurements from the TMP411 device included on the TMP411EVM. By default, once the EVM is connected and the GUI is loaded and running properly, the device starts converting and MCU starts reading the conversions which are automatically reported and displayed in the graph. On the right side of the graph, the user can also see the latest local and remote temperature read. The user can toggle visibility of specific line plots by clicking the corresponding item in the graph key.
The controls on the right side of the graph allow the user to easily configure the GUI and device settings, including:
Figure 3-4 Data Graph