SNOU211 November 2024
The perforation between the USB controller and TMP113 sensor breakout section is labeled on the bottom of the board on both sides for pin connections. Once the sensor section is detached from the controller section, the user can interface with the sensor section by soldering wires or 0.1'' header connectors. With this approach, the user has access to all 6 pins of the device.
Note that pullup resistors and protection diodes are on the controller section. Thus, when interfacing with other controller boards, TI recommends to verify that pullup resistors and protection circuitry are present on any controller board for safe and proper functionality.
Additionally, note that the default EVM configuration connects the ADDR pin to GND via the solderable jumper resistor. When interfacing the ADDR pin on the sensor breakout section to an external connection, remember to remove the jumper first to avoid shorting any pins. See Section 2.4 for more details.