SNOU211 November 2024
The Getting Started tab is used to set the target I2C address based on the ADDR pin connection. The default setting assumes that the ADDR pin is connected to GND. To change the I2C configuration, make the appropriate selection from the dropdown list. Then, click the button on the bottom left of the GUI to reinitialize communication.
Figure 3-3 Getting Started